Operation & Service Manual

PrimeLINE

and

PrimeLINE EDGE

Container Units

Manual Identification

Manual Number: T-372, Revision F

Models Covered: 69NT40-571-1xx and 69NT40-571-3xx

PIDs Covered: NT3xxx

Unit Controller: Micro-LINK ML5

Print Version: T-372 PDF version

Section 1: Safety Summary

The following general safety notices supplement specific warnings and cautions appearing elsewhere in this manual. They are recommended precautions that must be understood and applied during operation and maintenance of the equipment covered herein. Read More...

Section 2: Introduction

The Carrier Transicold PrimeLINE units are of lightweight aluminum frame construction, designed to be bolted onto the container front to serve as the container’s front wall. Forklift pockets are provided for installation and removal. Read More...

Section 3: Description

The container unit is designed so that the majority of components are accessible from the front. The unit model number, serial number and parts identification number can be found on the unit nameplate located next to the compressor. Read More...

Section 4: Microprocessor

The temperature control Micro-Link 5 microprocessor system consists of a controller (control module), display module, keypad and interconnecting wiring. The controller is fitted with power connectors, a micro USB port and short range wireless connectivity. Read More...

Section 5: Operation

Follow the procedures in the Operation section to inspect the unit, connect power, start and stop the unit, perform a pre-trip inspection and enable operating modes. Read More...

Section 6: Troubleshooting

The troubleshooting section includes probable causes for conditions affecting the unit from running properly, cooling and heating issues, abnormal pressures, noises, temperatures and other observable symptoms. Read More...

Section 7: Service

Container unit service procedures are provided to perform refrigerant service, maintain and replace components, and program the controller. Read More...

Section 8: Schematics

Electrical schematics and wiring diagrams are provided for three different unit configurations: PrimeLINE standard units, PrimeLINE standard units with EverFRESH, and PrimeLINE EDGE units (models 571-3xx models). Read More...

 

© Carrier Corporation 2024