Section 4
TROUBLESHOOTING
4.1Diesel Engine
4.1.1Engine
Will Not Start
Table
4–1 Engine
Will Not Start
Condition |
Possible
Cause |
Remedy
/ Reference Section |
Starter motor will not
crank or low cranking speed |
Battery insufficiently charged |
Charge |
Battery terminal post or battery defective |
Check |
Electrical connections at starter are
bad |
Correct |
Starter motor malfunctions |
Section 4.1.4 |
Starter motor solenoid defective |
Engine Manual |
Open starting circuit |
Section 4.1.5 |
Incorrect grade of lubricating oil |
Section 2.10 |
Fuse F5 is bad |
Replace |
Starter motor cranks,
but fails to start |
No fuel in tank |
Section
2.10 / Section 2.11. |
Air inside the fuel system |
Section 5.5.1 |
Water inside the fuel system |
Drain Sump |
Plugged fuel filters |
Replace |
Air intake heater is bad |
Section 5.5.14 |
Low oil / oil pressure switch defective |
Section 5.5.7 |
Faulty heater switch |
Section 5.5.15 |
Plugged fuel lines to injector(s) |
Engine Manual |
Mechanical lift fuel pump malfunction |
Engine Manual |
Fuses F1, F2, F3, F4 are bad |
Check/ replace |
Loose or no connection between wire
harness and Electronic Governor Module (EG) |
Check/correct |
Starter cranks and engages,
but dies after a few seconds |
Engine lube oil too heavy |
Section Section 2.10. |
Voltage drop in starter cable(s) |
Check |
4.1.2Engine
Starts Then Stops
Table
4–2 Engine
Starts Then Stops
Condition |
Possible
Cause |
Remedy
/ Reference Section |
Engine stops after a
few rotations |
No fuel in tank |
Section
2.10 / Section 2.11. |
Intake heater switch not held long enough |
Hold switch |
Fuel filter restricted |
Replace |
Air cleaner or hose restricted |
Section 5.5.11 |
Engine crankcase breather or hose restricted |
Section 5.5.12 |
Safety device open |
Section 2.9 |
Open wiring circuit to fuel solenoid |
Check |
Fuel solenoid defective |
Replace |
Fuel supply restricted |
Section 2.11,Section 5.5.2, and Section 5.5.3 |
Mechanical lift fuel pump malfunction |
Engine Manual |
Low oil / oil pressure switch defective |
Section 5.5.7 |
Leak in fuel system |
Check |
Injector nozzle(s) defective |
Engine Manual |
Injection pump defective |
Engine Manual |
Generator internal overloads open |
Table 2–4 |
4.1.3Engine
Will Not Shut Off
Table
4–3 Engine
Will Not Shut Off
Condition |
Possible
Cause |
Remedy
/ Reference Section |
Engine will not shut
off |
Loose ground connection |
Clean/Tighten |
Improperly seated fuel solenoid |
Correct |
4.1.4Starter
Motor Malfunction
Table
4–4 Starter
Motor Malfunction
Condition |
Possible
Cause |
Remedy
/ Reference Section |
Starter motor will not
crank or turns slowly |
Battery insufficiently charged |
Charge |
Battery cable connections loose or oxidized |
Check/Replace |
Battery cables defective |
Check/Replace |
Starter brushes shorted out |
Engine Manual |
Starter brushes hang up, defective or
have no contact |
Engine Manual |
Starter solenoid damaged |
Engine Manual |
Ignition switch defective |
Replace |
Engine lube oil too heavy |
Table 2.11. |
Starter motor turns,
but pinion does not engage |
Pinion or ring gear obstructed or worn |
Engine Manual |
Starter motor does not
disengage after switch has been released |
Ignition switch is bad |
Check/Replace |
Starter motor solenoid is bad |
Engine Manual |
Pinion does not disengage
after engine is running |
Starter is bad |
Engine Manual |
4.1.5Malfunction
In The Engine Starting Circuit
Table
4–5 Malfunction
In The Engine Starting Circuit
Condition |
Possible
Cause |
Remedy
/ Reference Section |
No power to starter motor
solenoid |
Battery defective |
Correct |
Loose electrical connections |
Tighten |
Fuel solenoid does not
energize or does not remain energized |
Battery defective |
Correct |
Loose electrical connections |
Tighten |
Oil pressure switch defective |
Section 1.9 |
Water temperature safety switch open |
Section 1.9 |
Fuel solenoid defective |
Engine Manual |
Intake heater switch is bad |
Check (Engine Manual) |
Electronic Governor Module (EG) is bad |
Replace (Section 5.5.14)
Check/Replace |
Intake heater does not
energize |
Intake heater switch is bad |
Section 5.5.14 |
Timer is bad |
Section 5.5.14 |
Heater element is bad |
Section 5.5.14 |
Heater relay is bad |
Section 5.5.14 |
4.1.6Miscellaneous Engine
Troubleshooting
Table
4–6 Miscellaneous
Engine Troubleshooting
Condition |
Possible
Cause |
Remedy
/ Reference Section |
Loss of power |
Restriction in air cleaner |
Section 5.5.11 |
Air in fuel system |
Section 5.5.11 |
Air vent restricted |
Clean |
Restricted fuel lines |
Engine Manual |
Fuel injection pump is bad |
Engine Manual |
Injector(s) bad or incorrect type used |
Engine Manual |
Incorrect fuel injection pump timing |
Engine Manual |
Incorrect valve timing |
Engine Manual |
Poor compression |
Engine Manual |
Vibration |
Engine shockmounts are bad |
Replace |
Poor compression |
Engine Manual |
Overheating |
Restriction in air cleaner |
Section 5.5.11 |
Exhaust pipe restriction |
Remove |
Restriction in water jacket |
Engine Manual |
Restriction in radiator |
Section 5.5.5 |
Coolant level too low |
Section 2.11. |
Loose water pump/alternator poly V-belt |
Section 5.5.10 |
Thermostat is bad |
Engine Manual |
Water pump is bad |
Engine Manual |
Excessive crankcase pressure |
Plugged crankcase breather line |
Section 5.5.12 |
4.2Battery
Charger (Solid State)
Table
4–7 Battery
Charger (Solid State)
Condition |
Possible
Cause |
Remedy
/ Reference Section |
CB4 trips when charger
is turned on |
Short in 12-volt wiring causing overload
of charger |
Locate and remove short or replace charger |
Circuit breaker trips
repeatedly, even when not connected |
Internal short |
Replace charger |
Charger does not taper
back after charging for a few minutes |
Bad cell in battery |
Test battery for defect according to
battery manufacturer’s instructions |
Charger is bad |
Replace |
Charger does not charge |
Open BCF3, BCF4, or BCF5 |
Replace |
Charger is not receiving AC input |
Use voltmeter to confirm charger is
receiving 360−500 VAC. If not, check input connections/fuses. |
Charger output is not connected to 12
volt battery |
Check output wiring connections to battery. |
Charger is bad |
Replace |
Low output voltage measured
across charger output |
Battery not connected to charger. It
is normal to measure 12 volts or less across charger output with
no battery connected |
Check charging leads from charger to
battery |
Reverse polarity connection
to battery has caused charger to stop charging |
Internal DC fuse blown and possible
damage to current carrying components |
Replace |
4.3Alternating
Current Generator
Table
4–8 Alternating
Current Generator
Condition |
Possible
Cause |
Remedy
/ Reference Section |
No voltage |
Loss of rotor magnetism |
Replace |
Circuit breaker tripped |
Check CB1 |
Open in stator windings |
Replace |
Short circuited |
Replace |
Worn drive gear stripped |
Check/Replace |
Contactor not engaged |
Replace |
Low voltage |
Low engine speed |
Section 5.5.12 |
High resistance connections, connections
are warm or hot |
Tighten |
Loss of rotor magnetism |
Replace |
Fluctuating voltage (May
be indicated by flickering lights) |
Fluctuating speed |
Section 5.5.12 |
Irregular speed of engine |
Engine Manual |
Loose terminal or load connections |
Tighten |
Bad bearing causing uneven air gap |
Replace |
High voltage |
Excessive engine speed |
Section 5.5.12 |
Overheating |
Generator overloaded |
Check |
Clogged vents / baffles |
Check/Clean |
High temperature surrounding generator |
Section 5.5.5 |
Insufficient air circulation or recirculation |
Check/Clean |
Unbalanced load |
Balance |
Dry bearing |
Replace |
Mechanical Noise |
Bad bearing |
Replace |
Rotor rubbing on stator |
Replace |
Loose laminations |
Replace |
Loose or misaligned coupling |
Check drive gear |
Generator frame produces
shock when touched |
Static charge |
Check ground to frame |
4.4Auto
Re-Start Option
Table
4–9 Auto
Re-Start Option
Condition |
Possible
Cause |
Remedy
/ Reference Section |
When the Ignition switch
is placed in the RUN position, nothing happens− no lights illuminate |
Wait 30 seconds for intake heater to
be activated |
Wait |
Relay defective |
Check/Replace |
Ignition switch defective |
Check/Replace Switch |
3 amp Fuse is bad |
Check and Replace Fuse |
Loose connector on module |
Tighten connector |
Auto restart module is bad |
Check for 12 volts at Pin 4/Replace
module |
Mis-wired connectors |
Check/Correct wiring |
Alarm sounds, but engine
does not crank |
No voltage at Pin 2 of the connector |
Trace/Correct |
Check Starter Solenoid |
Section 4.1.1 |
Auto restart module is bad |
Replace module |
Engine starts, but the
starter does not disengage |
Speed Sensor wiring loose |
Check/Correct |
Speed Sensor is bad |
Replace |
Auto restart module is bad |
Replace module |
Engine starts, but shuts
down from over speed |
Electronic Governor Module (EG) is bad |
Replace |
Engine cranks, but will
not start |
Electronic Governor Module (EG) is bad |
Replace |
Section 4.1.1 |
Section 4.1.1 |
Engine starts, but shuts
down on low oil |
Section 4.1.2 |
Section 4.1.2 |
Engine starts, but shuts
down on high water temperature |
Section
4.1.6 |
Section
4.1.6 |
4.5Electronic
Governor Module
Table
4–10 Electronic
Governor Modules
Fault |
LED
flash code |
Possible
Cause |
Engine Over Speed: more
than 2,530 RPM |
One Long - One Short |
ESS or mechanical engine problem |
Actuator Wiring Disconnection.
No signal from ESS for 2 seconds after RPM is greater than 1,000
RPM for 10 seconds, OR for 5 seconds while engine cranking (no
voltage at EG pin 18). |
Two Long - One Short |
Short ESS or wiring problem |
Speed Sensor Disconnection.
Fuel/speed actuator (FS) wiring disconnected or open circuit.
Coil Resistance Spec: 2.8 ohm +
10%. |
Two Long - Three Short |
FS or wiring problem |
EG supply voltage is
greater than 26V. |
Two Long - Seven Short |
EG or alternator problem |
4.6Voltage
Controller
The voltage controller has one green indicator light
and one yellow indicator light. When the green light is illuminated,
it means that the voltage controller is receiving power. The yellow light
only illuminates (flashes) to indicate that there is a problem.
Table
4–11 Voltage
Controller
Green
LED |
Fault |
Possible
Cause / Remedy |
LED not illuminated |
No power to the voltage controller |
Contactor failed |
Check line side power on contactors |
Yellow
LED flash Code |
Fault |
Possible
Cause / Remedy |
One Long - Three Short |
Over Voltage Error |
Engine speed, check |
One Long - Four Short |
Under Voltage Error |
Engine speed, check |