Section 3
3.1Refrigeration Unit - Front Section
The refrigeration unit is designed so that the majority of its components are accessible from the front (Figure 3.1). A manually operated venting system is located in the upper left access panel. Behind this left access panel are located the CO2 sensor and O2 sensor. The right access panel contains integrated components of the XtendFRESHTM Controlled Atmosphere option. This panel may be removed to allow entry into the evaporator section where the CO2 scrubber and other components are located.
Figure 3.1 Refrigeration Unit - Front
Components of the XtendFRESH option are mounted in the evaporator section in addition to the standard refrigeration unit components. These components (Figure 3.2) include the XtendFRESH Scrubber Assembly, Motor Assembly and Sensor Package.
Air from within the container is passed to the O2 sensor and CO2 sensor. Data is then supplied to the controller. The controller calculates O2 and CO2 values in order to maintain the preset values.
Figure 3.2 Evaporator Section Components
- - - - -
The AutoFRESH Interface Module (AIM) is a device that prevents the CO2 sensor from being calibrated when the ML3 controller is reset. The purpose of the device is to pull the CO2 sensor zero calibration line low when the CO2 sensor is calibrated.
The Ground Isolation Module (GIM) is a device installed on units with a scrubber motor that has the rotational output signal. The purpose of the module is to optically isolate the scrubber motor from the ML3 controller. Troubleshooting of this device is located in AL96 Troubleshooting table.
The Sensor Switch Module (SSM) is a device that allows for the O2 sensor and VPS sensor to use the same ML3 controller input. Controller software manages the switching of the device and reading of the correct input. Troubleshooting of this device is located in AL09 Troubleshooting table.
3.6Safety and Protective Devices
DEVICE |
DEVICE SETTING |
|---|---|
5 Amp |
|
Fuse FX3, FX4 - Time Delay |
15 Amp |
Fuse FX5, FX6 - Time Delay |
5 Amp |
Fuse FX7, FX8 (PIDs NT2709 and NT2774) |
5 Amp |