Section 4
|
Condition |
Possible Cause |
Remedy/Reference Section |
|---|---|---|
|
Starter motor will not crank or low cranking speed |
Battery insufficiently charged |
Charge |
|
Battery terminal post or battery defective |
Check |
|
|
Electrical connections at starter are bad |
Correct |
|
|
Starter motor malfunctions |
||
|
Starter motor solenoid defective |
Engine Manual |
|
|
Open starting circuit |
||
|
Incorrect grade of lubricating oil |
||
|
Fuse F5 is bad |
Replace |
|
|
|
|
|
|
Starter motor cranks, but fails to start |
No fuel in tank |
|
|
Air inside the fuel system |
||
|
Water inside the fuel system |
Drain Sump |
|
|
Plugged fuel filters |
Replace |
|
|
Air intake heater is bad |
||
|
Low oil / oil pressure switch defective |
||
|
Faulty heater switch |
||
|
Plugged fuel lines to injector(s) |
Engine Manual |
|
|
Mechanical lift fuel pump malfunction |
Engine Manual |
|
|
Fuses F1, F2, F3, F4 are bad |
Check/ replace |
|
|
Loose or no connection between wire harness and Electronic Governor Module (EG) |
Check/correct |
|
|
|
|
|
|
Starter cranks and engages, but dies after a few seconds |
Engine lube oil too heavy |
Section Section 2.10. |
|
Voltage drop in starter cable(s) |
Check |
4.1.2 Engine Starts Then Stops
4.1.3 Engine Will Not Shut Off
|
Condition |
Possible Cause |
Remedy/Reference Section |
|---|---|---|
|
Engine will not shut off |
Loose ground connection |
Clean/Tighten |
|
Improperly seated fuel solenoid |
Correct |
4.1.4 Starter Motor Malfunction
4.1.5 Malfunction In The Engine Starting Circuit
|
Condition |
Possible Cause |
Remedy/Reference Section |
|---|---|---|
|
No power to starter motor solenoid |
Battery defective |
Correct |
|
Loose electrical connections |
Tighten |
|
|
|
|
|
|
Fuel solenoid does not energize or does not remain energized |
Battery defective |
Correct |
|
Loose electrical connections |
Tighten |
|
|
Oil pressure switch defective |
Section 1.9 |
|
|
Water temperature safety switch open |
Section 1.9 |
|
|
Fuel solenoid defective |
Engine Manual |
|
|
Intake heater switch is bad |
Check (Engine Manual) |
|
|
Electronic Governor Module (EG) is bad |
Replace (Section 5.4.15) Check/Replace |
|
|
|
|
|
|
Intake heater does not energize |
Intake heater switch is bad |
|
|
Timer is bad |
||
|
Heater element is bad |
||
|
Heater relay is bad |
4.1.6 Miscellaneous Engine Troubleshooting
4.2 BATTERY CHARGER (SOLID STATE)
4.3 ALTERNATING CURRENT GENERATOR
4.5 ELECTRONIC GOVERNOR MODULE
The voltage controller has one green indicator light and one yellow indicator light. When the green light is illuminated, it means that the voltage controller is receiving power. During normal operations the yellow light is continuously blinking at a one Hz rate. If there is a problem then the yellow light will blink at various rates depending upon the fault. Refer to the chart below to determine the fault.
|
Green LED |
Fault |
Possible Cause/Remedy |
|---|---|---|
|
LED not illuminated |
No power to the voltage controller |
Contactor failed |
|
Check line side power on contactors |
|
Yellow LED flash Code |
Fault |
Possible Cause/Remedy |
|---|---|---|
|
One Long–Two Short |
Voltage Controller Fault |
Failed voltage controller, replace |
|
|
|
|
|
One Long–Three Short |
Over Voltage Error |
Engine speed, check |
|
|
|
|
|
One Long–Four Short |
Under Voltage Error |
Engine speed, check |
|
|
|
|
|
One Long–Five Short |
Hot Start Error |
Reset power to the unit |
|
|
|
|
|
One Long–Six Short |
Voltage Controller Fault |
Failed voltage controller, replace |
|
|
|
|
|
One Long–Seven Short |
Voltage Controller Fault |
Failed voltage controller, replace |
Electrical troubleshooting for high voltage control circuit
Before proceeding with the troubleshooting, make sure to follow your company’s standard safety procedures for working with electrical components.
|
ITEM |
CHECKS |
POTENTIAL CAUSE |
|---|---|---|
|
Receptacle (R) |
Check output voltage at Receptacle R (L1−L2, L2−L3, L1−L3) (50Hz: 360 − 460 VAC, and 60Hz: 400 − 500 VAC) |
Faulty Receptacle (Replace) |
|
High Voltage Wires (from Circuit Breaker to Receptacle) |
Check if wires/terminals are connected (Check Continuity for each leg) |
Loose connections (Tighten) |
|
Circuit Breaker (CB) |
Test the output power from Circuit Breaker CB (21−22, 22−23, 21−23) |
Faulty Circuit Breaker (Replace), Circuit Breaker (CB) is in the OFF position |
|
Verify Circuit Breaker (CB) is in the ON position |
||
|
Test the input power to the Circuit Breaker CB (11−12, 12−13, 11−13) |
||
|
High Voltage Wires (from Primary and Boost Contactors to Circuit Breaker, Voltage Controller, Fuse Blocks, Generator, and Battery Charger) |
Check if wires/terminals are connected (Check Continuity for each leg) |
Loose connections (Tighten) |
|
Primary (P) or Boost (B) Contactor |
Visually verify Primary (P) or Boost (B) Contactor is energized (wait 10−20 seconds after start−up) |
Faulty Contactor/Faulty Voltage Controller/Faulty Fuses/Faulty Generator (Replace) |
|
Test the output voltage from Primary (P) or Boost (B) Contactor (L1−L2, L2−L3, L1−L3) (50Hz: 360 − 460 VAC, and 60Hz: 400 − 500 VAC) |
||
|
Test the input voltage to Primary (P) or Boost (B) Contactor (T1−T2, T2−T3, T1−T3) (300 − 600 VAC) |
||
|
Test Voltage between terminals A1−A2 of Contactors. Engaged contactor (Primary or Boost) shall be supplied with ~24VDC; Dis−engaged 0VDC. |
if Not, check 24VDC circuit/Faulty Voltage Controller (Replace)if Not, check 24VDC circuit/Faulty Voltage Controller (Replace) |
|
|
Voltage Controller (VC) and Fuses |
Verify VCF6 Fuse is not blown (Check Continuity for each leg across fuse, outside of circuit; inside of circuit if not running) |
Blown Fuse (Replace) |
|
Verify VCF7 Fuse is not blown (Check Continuity for each leg across fuse, outside of circuit; inside of circuit if not running) |
Blown Fuse (Replace) |
|
|
Verify VCF1 Fuse is not blown (Check Continuity for each leg across fuse, outside of circuit; inside of circuit if not running) |
Blown Fuse (Replace) |
|
|
Verify VCF2 Fuse is not blown (Check Continuity for each leg across fuse, outside of circuit; inside of circuit if not running) |
Blown Fuse (Replace) |
|
|
Verify Voltage Controller has power (powered by high voltage) − verify green light is illuminated |
Faulty Voltage Controller, Blown VCF6 or VCF7 Fuse, Loose connections, Faulty Generator (Replace and tighten) |
|
|
Verify Voltage Controller has green light illuminated and yellow light flashing at 1 Hz (Yellow light flashing sequence other than at 1 Hz indicates a fault condition) |
One Long–Two Short = Voltage Controller Fault (Failed voltage controller, replace) |
|
|
One Long–Three Short = Over Voltage Error (Engine speed, check) |
||
|
One Long–Four Short = Under Voltage Error (Engine speed, check) |
||
|
One Long–Five Short = Hot Start Error (Reset power to the unit) |
||
|
One Long–Six Short = Voltage Controller Fault (Failed voltage controller, replace) |
||
|
One Long–Seven Short = Voltage Controller Fault (Failed voltage controller, replace) |
||
|
Verify that the Connectors to the Voltage Controller are secured (Snapped in place and do not easily pull out) |
Check if the connectors are pushed in all the way |
|
|
Remove connectors and inspect terminal pin insertion depth (all the same) |
||
|
Check to see if wires/terminals are connected (Check) |
||
|
Primary (P) or Boost (B) Contactor |
Visually verify Primary (P) or Boost (B) Contactor is energized (wait 10−20 seconds after start−up) |
Faulty Contactor/Faulty Voltage Controller/Faulty Fuses/Faulty Generator (Replace) |
|
Test the output voltage from Primary (P) or Boost (B) Contactor (L1−L2, L2−L3, L1−L3) (50Hz: 360 − 460 VAC, and 60Hz: 400 − 500 VAC) |
||
|
Test the input voltage to Primary (P) or Boost (B) Contactor (T1−T2, T2−T3, T1−T3) (300 − 600 VAC) |
||
|
Test Voltage between terminals A1−A2 of Contactors. Engaged contactor (Primary or Boost) shall be supplied with ~24VDC; Dis− engaged 0VDC. |
if Not, check 24VDC circuit/Faulty Voltage Controller (Replace) |