Section 9
|
|
__________-__________ Manufacturing Date: ___________
|
We, manufacturer: Carrier Transicold Pte Ltd
251 Jalan Ahmad Ibrahim
Singapore 629146
Declare, under our sole responsibility, that the PrimeLINE Container Unit:
Model: 69NT40-561 |
is in conformity with the provisions of the following European Directives:
• Machinery Directive 2006/42/EC following Annex VIII
• Electromagnetic Compatibility Directive 2014/30/EU following Annex II
• Radio Equipment Directive 2014/53/EU Annex II (with select options)
The assembly was assessed for applicability under the Pressure Equipment Directive, 2014/68/EU, but determined to be outside of the scope based on the exclusion indicated in PED Article 1, Paragraph 2.f. The assembly was determined to be no higher than PED Category I and is covered by the Machinery Directive 2006/42/EC.
The following Harmonized Standards were applied for this equipment:
Machinery Directive |
EMC Directive |
RED
Directive |
---|---|---|
EN ISO 12100:2010 EN 60204-1:2006 EN 13857:2008 |
EN 61000-6-2:2005 EN 61000-6-4:2007+A1:2011 EN55011:2009+A1:2010/CISPR11:2009+A1:2010 EN61000-4-2:2009 EN 61000-4-3:2006,+A1:2008, +A2:2010 EN 61000-4-4:2012 EN 61000-4-5:2006 EN 61000-4-6:2009 EN 61000-4-8:2010 EN 61000-4-11:2004 |
EN 61000-4-5:2006, EN 60950-1:2006, EN 62368-1:2014, EN 62311:2008, EN301 489-1 v2.1.1, EN 301 489-3 v2.1.1, EN 301 489-7 v1.3.1, EN 301 489-17 v3.2.1, EN 301 489-19 v2.1.1, EN 301 489-20 v2.1.1, EN 301 489-52 v1.1.0, EN 301 511 v12.5.1, EN 301 908-1 v11.1.1, EN 301 908-2 v11.1.2, EN 301 908-13 v11.1.2, EN 303 413 v1.1.1, EN 300 328 v2.2.1, EN 300 220-2 v3.2.1
|
The following Technical Standards were applied for this equipment:
•ISO 1496-2:2008
Person established in Europe authorized to compile a copy of the Technical File:
Shaun Bretherton
Service Engineering Manager of CTL Rotterdam
Pittsburgstraat 21 3047 BL Rotterdam
Netherlands