Section 4
TROUBLESHOOTING
4.1 DIESEL
ENGINE
4.1.1 Engine Will Not Start
Table 4–1 Engine
Will Not Start
Condition |
Possible
Cause |
Remedy/Reference
Section |
Starter
motor will not crank or low cranking speed |
Battery insufficiently
charged |
Charge |
Battery terminal
post or battery defective |
Check |
Electrical
connections at starter are bad |
Correct |
Starter motor
malfunctions |
Section 4.1.4 |
Starter motor
solenoid defective |
Engine Manual |
Open starting
circuit |
Section 4.1.5 |
Incorrect
grade of lubricating oil |
Section 2.10 |
Fuse F5 is
bad |
Replace |
|
|
|
Starter
motor cranks, but fails to start |
No fuel in
tank |
Section 2.10/Section 2.11. |
Air inside
the fuel system |
Section 5.5.1 |
Water inside
the fuel system |
Drain Sump |
Plugged fuel
filters |
Replace |
Air intake
heater is bad |
Section 5.5.14 |
Low oil /
oil pressure switch defective |
Section 5.5.7 |
Faulty heater
switch |
Section 5.5.15 |
Plugged fuel
lines to injector(s) |
Engine Manual |
Mechanical
lift fuel pump malfunction |
Engine Manual |
Fuses F1,
F2, F3, F4 are bad |
Check/ replace |
Loose or no
connection between wire harness and Electronic Governor Module
(EG) |
Check/correct |
|
|
|
Starter
cranks and engages, but dies after a few seconds |
Engine lube
oil too heavy |
Section Section 2.10. |
Voltage drop
in starter cable(s) |
Check |
4.1.2 Engine Starts Then Stops
Table
4–2 Engine Starts
Then Stops
Condition |
Possible
Cause |
Remedy/Reference
Section |
Engine
stops after a few rotations |
No fuel in
tank |
Section 2.10/Section 2.11. |
Intake heater
switch not held long enough |
Hold switch |
Fuel filter
restricted |
Replace |
Air cleaner
or hose restricted |
Section 5.5.11 |
Engine crankcase
breather or hose restricted |
Section 5.5.12 |
Safety device
open |
Section 2.9 |
Open wiring
circuit to fuel solenoid |
Check |
Fuel solenoid
defective |
Replace |
Fuel supply
restricted |
Section 2.11,Section 5.5.2, and Section 5.5.3 |
Mechanical
lift fuel pump malfunction |
Engine Manual |
Low oil /
oil pressure switch defective |
Section 5.5.7 |
Leak in fuel
system |
Check |
Injector nozzle(s)
defective |
Engine Manual |
Injection
pump defective |
Engine Manual |
Generator
internal overloads open |
Table 2–3 |
4.1.3 Engine
Will Not Shut Off
Table
4–3 Engine Will
Not Shut Off
Condition |
Possible
Cause |
Remedy/Reference
Section |
Engine
will not shut off |
Loose ground
connection |
Clean/Tighten |
Improperly
seated fuel solenoid |
Correct |
4.1.4 Starter Motor Malfunction
Table
4–4 Starter
Motor Malfunction
Condition |
Possible
Cause |
Remedy/Reference
Section |
Starter
motor will not crank or turns slowly |
Battery insufficiently
charged |
Charge |
Battery cable
connections loose or oxidized |
Check/Replace |
Battery cables
defective |
Check/Replace |
Starter brushes
shorted out |
Engine Manual |
Starter brushes
hang up, defective or have no contact |
Engine Manual |
Starter solenoid
damaged |
Engine Manual |
Ignition switch
defective |
Replace |
Engine lube
oil too heavy |
Table 2.11. |
|
|
|
Starter
motor turns, but pinion does not engage |
Pinion or
ring gear obstructed or worn |
Engine Manual |
|
|
|
Starter
motor does not disengage after switch has been released |
Ignition switch
is bad |
Check/Replace |
Starter motor
solenoid is bad |
Engine Manual |
|
|
|
Pinion
does not disengage after engine is running |
Starter is
bad |
Engine Manual |
4.1.5 Malfunction In The Engine
Starting Circuit
Table
4–5 Malfunction In The
Engine Starting Circuit
Condition |
Possible
Cause |
Remedy/Reference
Section |
No
power to starter motor solenoid |
Battery defective |
Correct |
Loose electrical
connections |
Tighten |
|
|
|
Fuel
solenoid does not energize or does not remain energized |
Battery defective |
Correct |
Loose electrical
connections |
Tighten |
Oil pressure
switch defective |
Section 1.9 |
Water temperature
safety switch open |
Section 1.9 |
Fuel solenoid
defective |
Engine Manual |
Intake heater
switch is bad |
Check (Engine
Manual) |
Electronic
Governor Module (EG) is bad |
Replace (Section
5.5.14)
Check/Replace |
|
|
|
Intake
heater does not energize |
Intake heater
switch is bad |
Section 5.5.14 |
Timer is bad |
Section 5.5.14 |
Heater element
is bad |
Section 5.5.14 |
Heater relay
is bad |
Section 5.5.14 |
4.1.6 Miscellaneous Engine Troubleshooting
Table
4–6 Miscellaneous Engine
Troubleshooting
Condition |
Possible
Cause |
Remedy/Reference
Section |
Loss
of power |
Restriction
in air cleaner |
Section 5.5.11 |
Air in fuel
system |
Section 5.5.11 |
Air vent restricted |
Clean |
Restricted
fuel lines |
Engine Manual |
Fuel injection
pump is bad |
Engine Manual |
Injector(s)
bad or incorrect type used |
Engine Manual |
Incorrect
fuel injection pump timing |
Engine Manual |
Incorrect
valve timing |
Engine Manual |
Poor compression |
Engine Manual |
|
|
|
Vibration |
Engine shockmounts
are bad |
Replace |
Poor compression |
Engine Manual |
|
|
|
Overheating |
Restriction
in air cleaner |
Section 5.5.11 |
Exhaust pipe
restriction |
Remove |
Restriction
in water jacket |
Engine Manual |
Restriction
in radiator |
Section 5.5.5 |
Coolant level
too low |
Section 2.11. |
Loose water
pump/alternator poly V-belt |
Section 5.5.10 |
Thermostat
is bad |
Engine Manual |
Water pump
is bad |
Engine Manual |
|
|
|
Excessive
crankcase pressure |
Plugged crankcase
breather line |
Section 5.5.12 |
4.2 BATTERY
CHARGER (SOLID STATE)
Table
4–7 Battery
Charger (Solid State)
Condition |
Possible
Cause |
Remedy/Reference
Section |
CB4
trips when charger is turned on |
Short in 12-volt
wiring causing overload of charger |
Locate and
remove short or replace charger |
|
|
|
Circuit
breaker trips repeatedly, even when not connected |
Internal short |
Replace charger |
|
|
|
Charger
does not taper back after charging for a few minutes |
Bad cell in
battery |
Test battery
for defect according to battery manufacturer’s instructions |
|
Charger is
bad |
Replace |
|
|
|
Charger
does not charge |
Open BCF3,
BCF4, or BCF5 |
Replace |
Charger is
not receiving AC input |
Use voltmeter
to confirm charger is receiving 360−500 VAC. If not, check input
connections/fuses. |
Charger output
is not connected to 12 volt battery |
Check output
wiring connections to battery. |
Charger is
bad |
Replace |
|
|
|
Low
output voltage measured across charger output |
Battery not
connected to charger. It is normal to measure 12 volts or less
across charger output with no battery connected |
Check charging
leads from charger to battery |
|
|
|
Reverse
polarity connection to battery has caused charger to stop charging |
Internal DC
fuse blown and possible damage to current carrying components |
Replace |
4.3 ALTERNATING
CURRENT GENERATOR
Table
4–8 Alternating Current
Generator
Condition |
Possible
Cause |
Remedy/Reference
Section |
No
voltage |
Loss of rotor
magnetism |
Replace |
Circuit breaker
tripped |
Check CB1 |
Open in stator
windings |
Replace |
Short circuited |
Replace |
Worn drive
gear stripped |
Check/Replace |
Contactor
not engaged |
Replace |
|
|
|
Low
voltage |
Low engine
speed |
Section 5.5.12 |
High resistance
connections - connections are warm or hot |
Tighten |
Loss of rotor
magnetism |
Replace |
|
|
|
Fluctuating
voltage (May be indicated by flickering lights) |
Fluctuating
speed |
Section 5.5.12 |
Irregular
speed of engine |
Engine Manual |
Loose terminal
or load connections |
Tighten |
Bad bearing
causing uneven air gap |
Replace |
|
|
|
High
voltage |
Excessive
engine speed |
Section 5.5.12 |
|
|
|
Overheating |
Generator
overloaded |
Check |
Clogged vents/baffles |
Check/Clean |
High temperature
surrounding generator |
Section 5.5.5 |
Insufficient
air circulation or recirculation |
Check/Clean |
Unbalanced
load |
Balance |
Dry bearing |
Replace |
|
|
|
Mechanical
Noise |
Bad bearing |
Replace |
Rotor rubbing
on stator |
Replace |
Loose laminations |
Replace |
Loose or misaligned
coupling |
Check drive
gear |
|
|
|
Generator
frame produces shock when touched |
Static charge
|
Check ground
to frame |
4.4 AUTO
RE-START OPTION
Table
4–9 Auto Re-Start
Option
Condition |
Possible
Cause |
Remedy/Reference
Section |
When
the Ignition switch is placed in the RUN position, nothing happens−
no lights illuminate |
Wait 30 seconds
for intake heater to be activated |
Wait |
Relay defective |
Check/Replace |
Ignition switch
defective |
Check/Replace
Switch |
3 amp Fuse
is bad |
Check and
Replace Fuse |
Loose connector
on module |
Tighten connector |
Auto restart
module is bad |
Check for
12 volts at Pin 4/Replace module |
Miswired connectors |
Check/Correct
wiring |
|
|
|
Alarm
sounds, but engine does not crank |
No voltage
at Pin 2 of the connector |
Trace/Correct |
Check Starter
Solenoid |
Section 4.1.1 |
Auto restart
module is bad |
Replace module |
|
|
|
Engine
starts, but the starter does not disengage |
Speed Sensor
wiring loose |
Check/Correct |
Speed Sensor
is bad |
Replace |
Auto restart
module is bad |
Replace module |
|
|
|
Engine
starts, but shuts down from over speed |
Electronic
Governor Module (EG) is bad |
Replace |
|
|
|
Engine
cranks, but will not start |
Electronic
Governor Module (EG) is bad |
Replace |
Section 4.1.1 |
Section 4.1.1 |
|
|
|
Engine
starts, but shuts down on low oil |
Section 4.1.2 |
Section 4.1.2 |
|
|
|
Engine
starts, but shuts down on high water temperature |
Section 4.1.6 |
Section 4.1.6 |
4.5 ELECTRONIC
GOVERNOR MODULE
Table
4–10 Electronic Governor
Modules
Fault |
LED
flash code |
Possible
Cause |
Engine
Over Speed: more than 2,530 RPM |
One Long–One
Short |
ESS or mechanical
engine problem |
|
|
|
Actuator
Wiring Disconnection. No signal from ESS for 2 seconds after RPM
is greater than 1,000 RPM for 10 seconds, OR for 5
seconds while
engine cranking (no voltage at EG pin 18). |
Two Long–One
|
Short ESS
or wiring problem |
|
|
|
Speed
Sensor Disconnection. Fuel/speed actuator (FS) wiring disconnected
or open circuit. Coil Resistance Spec: 2.8 ohm +/- 10%. |
Two Long–Three
Short |
FS or wiring
problem |
|
|
|
EG
supply voltage is greater than 26V. |
Two Long–Seven
Short |
EG or alternator
problem |
4.6 VOLTAGE
CONTROLLER
The voltage controller has one green indicator light
and one yellow indicator light. When the green light is illuminated,
it means that the voltage controller is receiving power. The yellow light
only illuminates (flashes) to indicate that there is a problem.
Table
4–11 Voltage
Controller
Green
LED |
Fault |
Possible
Cause/Remedy |
LED
not illuminated |
No power to
the voltage controller |
Contactor
failed |
Check line
side power on contactors |
Yellow
LED flash Code |
Fault |
Possible
Cause/Remedy |
One
Long–Two Short |
Voltage Controller
Fault |
Failed voltage
controller, replace |
|
|
|
One
Long–Three Short |
Over Voltage
Error |
Engine speed,
check |
|
|
|
One
Long–Four Short |
Under Voltage
Error |
Engine speed,
check |
|
|
|
One
Long–Five Short |
Hot Start
Error |
Reset power
to the unit |
|
|
|
One
Long–Six Short |
Voltage Controller
Fault |
Failed voltage
controller, replace |
|
|
|
One
Long–Seven Short |
Voltage Controller
Fault |
Failed voltage
controller, replace |